This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Buffer contain maximum how many request of 80 byte each in A2530E24C module with spi communication

Other Parts Discussed in Thread: MSP430F5310

Hi All,

                       I am using A2530E24C module with preloaded Anaren ZNP firmware in it. I am communicating Anaren chip with MSP430F5310 via spi . As I am sending total 15 request of each 80 bytes from Coordinator to Router device. On Router device i found that 15 request  will be pending in its buffer module until one cannot  read. I want to know buffer contain maximum how many request of 80 byte each. Thanks for your co-operation.

Regards,

Ronak Jain,

  • Ronak ,
    Can you pls explain the issue in more detail - do you have 2 or more A2530E24C acting as cooridnator and routers or do you have cc2530EMs (or other devices) as well ? When the bytes in Rx FIFO cross a certain threshold, router should read the frame bytes from the FIFO. Is the router not reading the frame after receiving certain number of pkts ?

    Saurabh
  • I have test using only 2 A2530E24C chip ( 1 as coordinator & second as router ). Yes when i have send 20 request of 80 bytes each , then router is not reading all 20 request ,router reads only 15 request from FIFO. So i want to know that Rx FIFO buffer accomodate maximum how many request.