Other Parts Discussed in Thread: CC2530, Z-STACK
Hello
I run my coordinator on CC2530 with the ZNP firmware. Currently routing is done with standard AODV.
To support larger networks, I might have to switch to MTO / Source routing, with the routes stored in the host application and the coordinator being the concentrator.
- Do I need to compile the ZNP code with a special flag for this?
- Using ZNP, is the "host" or the "ZNP firmware" responsible for sending the RouteDiscoverRequests?
- If RouteDiscoveries are initiated by the host application (which would make sense, I guess), which ZNP/Z-Tool request sends this RouteDiscoveryRequest?
Thanks fro your answers
Philipp