Other Parts Discussed in Thread: CC2538, CC2530, CC2520, MSP430F5438A
Hi Friends,
I am using custom board and zstack SampleApp application for my project.
When I have downloaded the code into msp430, the ieee address location is erased.
I can view the IEEE address using z tool. it always returns 0xFF in all 8 byte.
So that I have written the IEEE address using z tool.
For using z tool, I have enabled the below compile options.
ZTOOL_P1
MT_TASK
MT_SYS_FUNC
MT_ZDO_FUNC
But I have used the UART(using polling method) for displaying some of my information onto the teraterm.
1) If i want to use z tool for configuring IEEE address, I will add above compile options, follow interrupt based uart code and teraterm console display some garbage values.
2) Also Anyone can connect my device using z tool and access some information.
So,
Is there any way to configure the IEEE address other than using z tool after downloaded the code into target?
Regards,
Keerthi G.