Other Parts Discussed in Thread: Z-STACK
when i rebuild the project,that comes a problem,my IAR is 8.30.2,but the project is creat from ZStack-CC2530-2.3.0-1.4.0 by IAR8.10.2,the problem is as follow:
Error[e16]: Segment RAM_CODE_FLASH (size: 0x27 align: 0) is too long for segment definition. At least 0x4 more bytes needed. The problem occurred
while processing the segment placement command "-Z(CODE)RAM_CODE_FLASH=_RAM_CODE_FLASH_START-_RAM_CODE_FLASH_END",
where at the moment of placement the available memory ranges were "CODE:39ddd-39dff"
Reserved ranges relevant to this placement:
CODE:39ddd-39dff RAM_CODE_FLASH
BIT:0-7 BREG
BIT:80-97 SFR_AN
BIT:a0-af SFR_AN
BIT:b8-c7 SFR_AN
BIT:d8-df SFR_AN
BIT:e8-ef SFR_AN
Who can hlep me solve the problem,thanks!