Hi
we want to design an RF gateway used to collect Zigbee and 6lowpan frames in parallel and in simultaneous way from diffrent devices technology (Zigbee, 6lowpan).
we have to work on the 2.4GHz band for both protocols. we re trying to find the best solution hw / sw to reply to this need.
1- One RF interface CC2520 + 2 MSP430 (MSP1 for Zigbee; MSP2 for 6lowpan), then frames will be routed to the main MCU via SPI
==> complexity on sw routing and filtering frames ?!
2- Two separeted modules ( with 2antenna) : CC2530 (Zigbee) and another CC2530 (6LoWPAN)
==> due to the same band, can we get interference problems in this situation ?!
any remarks ? is there any other suggestion ?
thanks