Other Parts Discussed in Thread: Z-STACK
Here is source code of a library (hal_types.h) that is used in ZigBee Mesh stack that is released by TI.
#ifndef HAL_TYPES_H_
#define HAL_TYPES_H_
/* ------------------------------------------------------------------------------------------------
* Types
* ------------------------------------------------------------------------------------------------
*/
typedef signed char int8;
typedef unsigned char uint8;
typedef signed short int16;
typedef unsigned short uint16;
typedef signed long int32;
typedef unsigned long uint32;
typedef unsigned long long uint64;
typedef uint32 halDataAlign_t;
#define bool _Bool
/* ------------------------------------------------------------------------------------------------
* Compiler Macros
* ------------------------------------------------------------------------------------------------
*/
/* ----------- IAR Compiler ----------- */
#ifdef __IAR_SYSTEMS_ICC__
#define ASM_NOP asm("NOP")
/* ----------- KEIL Compiler ---------- */
#elif defined __KEIL__
#define ASM_NOP __nop()
/* ----------- CCS Compiler ----------- */
#elif __TI_COMPILER_VERSION
#define ASM_NOP asm(" NOP")
/* ----------- GNU Compiler ----------- */
#elif defined __GNUC__
#define ASM_NOP __asm__ __volatile__ ("nop")
/* ---------- MSVC compiler ---------- */
#elif _MSC_VER
#define ASM_NOP __asm NOP
/* ----------- Unrecognized Compiler ----------- */
#else
#error "ERROR: Unknown compiler." //LINE 63!!!!!!!!!
#endif
/* ------------------------------------------------------------------------------------------------
* Standard Defines
* ------------------------------------------------------------------------------------------------
*/
#ifndef TRUE
#define TRUE 1
#endif
#ifndef FALSE
#define FALSE 0
#endif
#ifndef NULL
#define NULL 0
#endif
/* ------------------------------------------------------------------------------------------------
* Memory Attributes
* ------------------------------------------------------------------------------------------------
*/
#define XDATA
#define CODE
#endif /* HAL_TYPES_H_ */
I use CCS v6.0.1.00040 and TI v5.1.6 as the compiler. When I hit the compile button on CCS, I get this error
"..\hal_types.h", line 63: fatal error #35: #error directive: "ERROR: Unknown compiler."
I don't get any error when I replace line 63 with " #define ASM_NOP asm(" NOP") ". Could anyone tell me why the compiler does not recognize the
"#elif __TI_COMPILER_VERSION" line?