Other Parts Discussed in Thread: Z-STACK, CC2530
How can I remove offline(unknown or obsolete) node in a remote router's assocdevlist?
I am working on home automation system. Generally there is a gateway device with ZNP module as a ZigBee coordinator. Serveral router or enddevice radios integrated on controllable or reporting device (such as lamp, sensor, switch etc.). The problem is found in my testing setup and I believe it will be also a issue in future production stage.
Okay, the following are the details. When ZNP is started up, 1 or more (assume 3 and numberred 1, 2, 3) router device may join the PAN formed by ZNP. So 1 coordinator and 3 routers are in the current ZigBee network. And assume there is a situation that router 1 is close to ZNP and just associated with ZNP directly. But router 2 and 3 have some distance from ZNP, so they are both joined the network as children of router 1. The network topology is actually very simple. ZNP has one child which is router 1 and router 2 has two children which are router 2 and 3. Then for some reason, router 3 is just powered down and never powered back as a normal ZigBee device. The the issue comes, router 3 is always existed in the assocdevlist of router 2. Everytime when the gateway application performs device discovery with IEEE_ADDR_REQ there is no response from the router 3 (because it doesn't existed in the network anymore, I call it offline or obsolete). Worse than that, if there are too many offline or obsolete devices, router 2 may not accept new joining device. That means those offline devices occupy the assocdevlist space in router 2.
So the question is how to remove theose obsolete node(s) from assocdevlist in a remote device (always router type)?
I considered some possible solutions but not reasonable under all conditions.
(1). Send ZdoMgmtLeave request, but this request needs a known IEEE Address. IEEE address may be looked up through Z-Stack Address Manager when access ZNP directly. That means we may get the IEEE address of device in the assocdevlist on ZNP but not other remote router device in network.
(2). Send MGMT_LQI_REQ to discover device in network instead of sending IEEE_ADDR_REQ. Yes, this may avoid waiting response from offline device(s). But it doesn't solve the issue that router 2 may not accept new joining if its assocdevlist is full of obsolete devices.
Could anyone figure me out how to implement a workable solution? All I description is based on Z-Stack Home 1.2.1 and CC2530 radio (ZNP or devices).