Other Parts Discussed in Thread: CC2531, CC2591, CC2530
Hello everyone! I use to enhance the distance cc2531 of cc2591, and hardware design is:
Coordinator : cc2531 + cc2591 ( cc2591 CC2531)
PAEN P0_7
EN P1.4
HGM P1_1
End Device :Only cc2530
After Communication, coordinator transmission distance is increased by about 200m. But receive no change and the distance only 10m.
How do I fix?