Other Parts Discussed in Thread: CC2538, CC2538-CC2592EMK, CC2592
I unable to communicate between two cc2538-cc2592 modules with one as coordinator and other router, but if i use one cc2538 module as coordinator or router, i am able to communicate with the cc2538-cc2592 module. It is just the combination of two cc2538-cc2592 modules which is not working.
I am using GenericApp example code for sending data between the two. I can not see any other setting in Z stack required specifically for cc2538-cc2592 EMK.
Is there anything i am missing out here?