Other Parts Discussed in Thread: CC2530
Hello,
Now I'm up against a problem of downloading to CC2530 by ccDebugger.
Firstly i tried to download HEX file into SmartRF05 Evaluation Board Rev. 1.7.1 on which CC2530 EM discrete 1.3.1 is mounted using cc Debugger and SmartRFR Flash Programmer.
But I couldn't write and after it even only with SmartRFR Flash Programmer via USB download became disable.
I gave up to use the SmartRF05 Evaluation Board Rev. 1.7.1 and I started to try to write into my original CC2530 board not so different with CC2530 EM discrete 1.3.1.
But error occurred with following message.
CC2530 - ID5697: Error in HEX file verification
Though cc Debugger itself seems to be recognized showing info in upper window.
EBID:5697 Chip type:CC2530 EB type CC Debugger EB firmware: 05CC EB firmware rev: 0008
If there are someone know how to solve, please show me.
Thanks