Other Parts Discussed in Thread: MSP430F5438, TIMAC, CC2531EMK
hai i am using the cc2520-2591 emk when i configure the chip and simply load the data in the txfifo buffer in one board and transmit the data.on the other side by disabling the frame filter enable bit FRMFILT0.FRM_FILTER_EN and i start receiving the data on the other board i get the same data what i was transmitting is received on the rxfifo buffer .
i want to know the IEEE802.15.4 frame format details
and the local address information that is SHORT_ADDR ,PAN_ID,EXT_ADDR
and Source address matching control.