This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2538 - Source files to recompile the libraries TIMAC-CC2538.a and Router.a

Other Parts Discussed in Thread: CC2538, Z-STACK

Hi, 

I need to understand why the signal strength on the stack ZigBee Smart Energy 1.1.0 for cc2538 is set to 0 dBm while we need to be 7 dBm.

The problem is that it has routines of MAC layers that are available through the libraries  TIMAC-CC2538.a and Router.a, like to have access to the source files, such as mac_api.c.
Where can I download these files to include in the project and recompile libraries TIMAC-CC2538.a and Router.a ?
Thank you,