This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2538 ZStack low power mode wake-up delay

Hi All,

I have checked the forum and there does not seem to be an article that deals with this problem:

I have a development using the ZStack Energy 1.1.0's IPD base.

I have added 8 buttons to it on port C, to do something. I use an ISR and the low power modes quite successfully. We get to LPM 2 and possibly 3, and it wakes up quickly with no problems when the power interrupt type is set to GPIO_POW_FALLING_EDGE, with the function GPIOPowIntTypeSet() .  

One of my requirements is to have it wake up from the rising edge. If I use GPIO_POW_RISING_EDGE, there is a delay of up to 3 seconds, between the pin signal rising up, and the ISR being entered with assigned task being performed. Is there a way to fix this, and have it enter the ISR instantly?

Some detail:

Within the ISR, I test the state of the pin that triggered the ISR, and change between GPIO_POW_RISING_EDGE and GPIO_POW_FALLING_EDGE as follows:

if ( newSwitchStates & 0x01 )   {     //If HIGH, then next trigger will need FALLING edge; if LOW, then RISING edge..
  GPIOPowIntTypeSet(GPIO_C_BASE, GPIO_PIN_0, GPIO_POW_FALLING_EDGE );  }
else  {
  GPIOPowIntTypeSet(GPIO_C_BASE, GPIO_PIN_0, GPIO_POW_RISING_EDGE );  }  }

Any tips would be greatly appreciated.

Thanks & Regards, DanO.