Other Parts Discussed in Thread: CC2530, CC2630
Hi everyone,
there is a question of the CC2530 actual power comsumption.
as we know ,zstack support the powersaving , and it will be as low as 1uA in ideal state.
but when it open the RF ,not only sending the warning msg and recevie remote data ,it cost more than 20mA,
although that is configurable, but it aslo cost mA
so there is a problem while CC2530 used in the actual products.
we can imagine that a connect switch which install on the door,
it will not only wake up to sending warning msg when door open but also poll his parents every 60s (Zigbee profile recommended)
so as a customer,i do have doubt about whether zigbee is fit for powering by battery ?
how could we control the customer do not open and close the door frequently!!!!!!