I am researching the use of the CC2650 6LoWPAN in a sensor network solution and had a few questions.
1. What is the maximum number of nodes that each mesh network can support...would 1500 be possible? What are the recommendations?
2. What is the maximum number of nodes that each edge router can support...again is 1500 possible?
3. Will the nodes still be able to run on batteries for extended periods? Each node will have 1 simple sensor and likely update rate of around 1 sample a minute maximum...perhaps less.
4. Can 6LoWPAN work with more than 1 edge router...so you have some form of redundancy?
5. Are there any 6LoWPAN (over 2.4GHz) to Wi-Fi Edge Router available on the market? or is their any software or reference designs available for this?
Thanks, any questions that can be answered would be of a great help!
Glenn.