This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Monitor Test and Connect Ztool "No device connect"

Other Parts Discussed in Thread: CC2530, CC2530EM

I use CC2530 soc

Hex file build from HomeAutomation: SampleSwitch. I can't connected Ztool

Symbols Preprocessor: 

SECURE=1
TC_LINKKEY_JOIN
xNV_INIT
xNV_RESTORE
xHOLD_AUTO_START
ZTOOL_P1
MT_TASK
MT_APP_FUNC
MT_SYS_FUNC
MT_ZDO_FUNC
xLCD_SUPPORTED=DEBUG
MULTICAST_ENABLED=FALSE
ZCL_READ
ZCL_WRITE
ZCL_REPORT
ZCL_EZMODE
ZCL_BASIC
ZCL_IDENTIFY
ZCL_ON_OFF
ZCL_DIAGNOSTIC
FEATURE_SYSTEM_STATS
HAL_UART
HAL_UART_DMA=1
HAL_UART_ISR=0
xHAL_UART_ISR_TX_MAX
xLCD_SUPPORTED
HAL_DMA=TRUE
MT_ZDO_CB_FUNC
MT_ZDO_MGMT
ZAPP_P1

UART Config:

PORT 0 , Baud: 38400, Flowcontrol: FALSE...  connect with RS232 pin 2,3,5 with P0_2,P0_3 and ground

Plz help me

Tks