Other Parts Discussed in Thread: Z-STACK
Dears,
If I want to implement a Zigbee HA bulb, Is it possible to send OTA message to factory reset a HA devices? this is because there shouldn't have physical button on bulb so we need this.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: Z-STACK
Dears,
If I want to implement a Zigbee HA bulb, Is it possible to send OTA message to factory reset a HA devices? this is because there shouldn't have physical button on bulb so we need this.
To the best of my knowledge, there is nothing in the spec that says how factory reset should be performed. If so, I think it is vendor dependent.
Now, a bulb is either factory new or joined to a network.
If it is in a network, then it could can reset in two ways :
a) From another device in the network by sending a zdo.leave (something like that) to ask the bulb leave , the bulb can take that as a trigger to reset itself
b) From a device outside of the network that perform a ZLL touchlink -> factory reset procedure
As far as I know, you can do that on ge link, cree, philips bulbs.
Yes ZLight programmed with ZStack-Lighting1.0.2 does support a Factory Reset command. However there are 2 differences in resetting ZLight vs off the shelf ZLL devices.
1. Zlight will NOT accept a TouchLink command from a device advertising a Key Bit Mask with ZLL Master Key. It requires the Certification bit to be set for it to respond to the touchlink scan request.
What device are you using to reset the Philips / GE devices? As these devices are using the ZLL Master Key the same will not reset a ZLight. If the device doing the reset is built with ZStack-Lighting-1.0.2 then you can change the key bit mask in zll.h by changing the ZLL_KEY_INDEX:
// For production: //#define ZLL_ENC_KEY ZLL_MASTER_KEY //#define ZLL_LINK_KEY ZLL_MASTER_LINK_KEY //#define ZLL_KEY_INDEX ZLL_KEY_INDEX_MASTER // For certification only: #define ZLL_ENC_KEY ZLL_CERTIFICATION_ENC_KEY #define ZLL_LINK_KEY ZLL_CERTIFICATION_LINK_KEY #define ZLL_KEY_INDEX ZLL_KEY_INDEX_CERT
The ZLL_ENC_KEY and ZLL_LINK_KEY do not need to be set correctly as the touchlink reset does not use them (this is why an uncertified device can reset a certified device).
2. TouchLink is proximity based. The Touchlink RSSI filter in ZLight is "strict" meaning that you may need to be closer for the touchlink to work.
This can be changed in zll.h or in project options by changing ZLL_TL_WORST_RSSI:
// Manufacturer specific threshold (greater than -128), // do not respond to Touch-link scan request if reached #ifndef ZLL_TL_WORST_RSSI #define ZLL_TL_WORST_RSSI -40 // dBm #endif
Regards, TC.
Slight correction.
TopCat said:1. Zlight will NOT accept a TouchLink command from a device advertising a Key Bit Mask with ZLL Master Key. It requires the Certification bit to be set for it to respond to the touchlink scan request.
It is actually the remote that will not accept the scan response and send the identify if the keybit in the scan response does not match a bit in its key bit mask. The ZLL_KEY_INDEX must be changed on the remote and not the light.
Regards, TC.