Hi,
I was working with the Transmit App application with Z-Stack, and was able to achieve a throughput of about 104kbps (between coordinator and router). I tried connecting a few more routers to the Coordinator, and tested the throughput. The throughput per node fell to half, which is expected. However, when I tried connecting 3 nodes to the coordinator and used Transmit App, the throughput on two devices fell to 0, and the third one was 32 Kbps.
I realize that Transmit App was built for a point to point network. But, is there a rule of thumb that I can follow for the decrease in Throughput due to the number devices connected to the Coordinator (or any Router in general)?
Thanks in advance,
SF