Firstly i'm very new to 6LoWPAN, and trying to get my head around it, so if the questions seem a little odd, please forgive me.
I'm currently working on another project with a TI CC3200 and a CC2650, where the intention is to provide a Wifi --> Bluetooth Gateway.. The issue that i'm likely to face is that i'll only be able to connect to a few devices at the same time. ( max 3)..
It struck me that the CC2650 can run other protocols and i thought that just maybe we might be able to to use this same bridge as a way to connect to many more devices..
Could the 2650 be used as the 6LoWPAN edge router ( if its connected to something more powerful, like a CC3200 ). In the Contiki-6LOWPAN wiki, i see that a Beaglebone and CC2531 is used. This is a possible option, but not nessarily ideal..
I'm hopeful someone can provide some guidance.