Dear all,
I am working on this small device which is powered up using Henlv AC-to-DC PSU.
I notice that the CC2530 modules will auto-RESET if we are doing fast I/O port on/off. What might have cause this problem?
What we have tried:
1. We have tried changing capacitor at the RESET Pin to bigger cap and also added series resistors to reduce noise - no improvement.
2. We notice our circuit is drawing 446uA from the P0.5 and P0.1, we add a resistor to both pin to reduce current drawn to less than 4mA - still no improvement.
Need help and advice. Thanks.