Other Parts Discussed in Thread: CC2531, Z-STACK
Hi,
I am getting the below error when I am trying to build the "SampleLight" Project for ZLL Zlight2 for CC2531 Evaluation Kit:
Error[e46]: Undefined external "?V1" referred in AF ( C:\Texas Instruments\Z-Stack Lighting 1.0.2\Projects\zstack\ZLL\SampleApp\CC253x\EndDeviceEB\Obj\AF.r51
My IAR Details are:
IAR Assembler for 8051
8.30.1.41636 (8.30.1.41636)
IAR C/C++ Compiler for 8051
8.30.1.41636 (8.30.1.41636)
Can you please let me know if I am missing anything.
By searching online, I got the below link:
www.deyisupport.com/.../124362.aspx
It has a chipcon_cstartup.s51 file, which it asks to replace with the existing chipcon_cstartup.s51 file.
I tried to diff and I saw that the new file has 8 Virtual Registers mentioned. So is it safe to replace the above mentioned file ?
I replaced the above file, and changed the "Number of Virtual Registers" to "8". The code got compiled, but I need some confirmation before I flash the code in the Light2 HW.
Awaiting your reply.
Thanks,
Sunny