This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2538NF11 icf File

Hi,

I am trying to download code to a custom board based on the CC2538EM but with a CC2538NF11 chip instead of the CC2539SF53. I am using the XDS100v3 on my SmartRF, however I think the linker configuration file (*.icf) is incorrect. I have set the device type to the NF11 in IAR but I think the linker file they provide isn't working. Here is its contents:

/*###ICF### Section handled by ICF editor, don't touch! ****/
/*-Editor annotation file-*/
/* IcfEditorFile="$TOOLKIT_DIR$\config\ide\IcfEditor\cortex_v1_0.xml" */
/*-Specials-*/
define symbol __ICFEDIT_intvec_start__ = 0x00200000;
/*-Memory Regions-*/
define symbol __ICFEDIT_region_ROM_start__ = 0x00200000;
define symbol __ICFEDIT_region_ROM_end__ = 0x0021ffd3;
define symbol __ICFEDIT_region_RAM_start__ = 0x20000000;
define symbol __ICFEDIT_region_RAM_end__ = 0x20003fff;
/*-Sizes-*/
define symbol __ICFEDIT_size_cstack__ = 0x800;
define symbol __ICFEDIT_size_heap__ = 0x1000;
/**** End of ICF editor section. ###ICF###*/

//
// Define a memory region that covers the entire 4 GB addressible space of the
// processor.
//
define memory mem with size = 4G;

//
// Define a region for the on-chip flash.
// This device has 128KB Flash size
//
define region FLASH = mem:[from __ICFEDIT_region_ROM_start__ to __ICFEDIT_region_ROM_end__];

//
// Define a region for Customer Configuration Area in flash.
//
define region FLASH_CCA = mem:[from 0x0021ffd4 to 0x0021ffdf];

//
// Define a region for the on-chip SRAM.
// This device has 16KB RAM size
//
define region SRAM = mem:[from __ICFEDIT_region_RAM_start__ to __ICFEDIT_region_RAM_end__];

//
// Define regions of retention and non-retention RAM. This device has only
// the RAM block with retention.
//
define region SRAM_RETENTION = mem:[from __ICFEDIT_region_RAM_start__ to __ICFEDIT_region_RAM_end__];

//
// Define a block for the heap. The size should be set to something other
// than zero if things in the C library that require the heap are used.
//
define block HEAP with alignment = 8, size = __ICFEDIT_size_heap__ { };

//
// Indicate that the read/write values should be initialized by copying from
// flash.
//
initialize by copy { readwrite };

//
// Indicate that the noinit values should be left alone.
//
do not initialize { section .noinit };

//
// Place the interrupt vectors at the start of flash.
//
place at address mem:__ICFEDIT_intvec_start__ { readonly section .intvec };

//
// Place the cca area at the end of flash (start of FLASH_CCA).
//
place at start of FLASH_CCA { readonly section .flashcca };

//
// Place the remainder of the read-only items into flash.
//
place in FLASH { readonly };

//
// Place the RAM vector table at the start of retention ram.
//
place at start of SRAM_RETENTION { section VTABLE };

//
// Place all read/write items into retention SRAM.
//
place in SRAM_RETENTION { readwrite, block HEAP };

//
// Define CSTACK block to contain .stack section. This enables the IAR IDE
// to properly show the stack content during debug. Place stack at end of
// retention RAM, do not initialize (initializing the stack will destroy the
// return address from the initialization code, causing the processor to branch
// to zero and fault)
//
define block CSTACK with alignment = 8, size = __ICFEDIT_size_cstack__ { section .stack };
do not initialize { section .stack };
place at end of SRAM_RETENTION { block CSTACK };

//
// Export stack top symbol. Used by startup file.
//
define exported symbol STACK_TOP = __ICFEDIT_region_RAM_end__ + 1;

//
// Variables that do not need retention should be defined here
// Only retention RAM on this device variant
place in SRAM_RETENTION { section .nonretenvar };

Could anyone verify if this file should work, and if not provide the correct version?

Thanks in advance,

Brendon