This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Packet time ZC-ZED (END-TO-END) very long. Why?

Other Parts Discussed in Thread: CC2538

I'm oscilloscope measuring some times to get an idea which dataspeed is feasible. I'm using the ZNP images for all nodes.

For a single link ZC-ZR vs. ZC-ZED I see a huge difference.

For the ZC-ZR I measure an average 80 bytes package time (with END-TO-END acknowledge) of ~30ms.

The ZC-ZED is unusable slow and varies a lot! 150ms up to 500ms

What's going on?

Any thoughts to improve this are very welcome