This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2592 Range Extender Interface with MCR20AVHM ZigBee transceiver

Other Parts Discussed in Thread: CC2592

Hello TI Team,


We are interfacing CC2592 with one of the freescale MCR20AVHM ZigBee transceiver chip. The problem with the interface lies in both Transmit and Receive mode. In both these mode, we are able to get data in only 50% of cases. For CC2592 transmit mode, PA_EN = 1, LNA_EN = 0 and HGM = 1 (HGM can be 0/1 as per CC2592 datasheet in transmit mode) and CC2592 receive mode configuration is PA_EN = 0, LNA_EN = 1 and HGM = 1.


FYI...we are able to get small spike (in microseconds) on PA_EN line when MCR20AVHM transmits data.


Is there any special requirement in interfacing CC2592 with MCR20AVHM? Schematic snapshot is attached for your reference.