This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Unknown MT_APP Command

I am running OTA_Dongle as coordinator, there is no router in network.

When I power coord on, it sends following message continuosly to host:

0A:09:00:14:8A:00:11:20:00:00:0E:14:09

Which is a POLL APP command, but I can't see it in MT API doc. Can you help what is this message?

Thanks.