This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2531 Which Firmware should I use

Other Parts Discussed in Thread: CC2531, CC2538, REMOTI, TIMAC, Z-STACK

Hello everyone,

I have a CC2531 which currently is being used as a RF packet sniffer.  I now need to use this USB dongle as a central node of the system.  I have already talked to the semiconductor help and he suggested I post here.  

My end goal is to be able to be able to use the USB port to write packets out to a specific node (CC2538)  and read packets from different CC2538 nodes.  

As far as I can see there are three options:

RemoTI

TIMAC  

ZStack

Semiconductor help suggested that TIMAC might work but he was not 100% sure.  

My end goal is to be able to be able to use the USB port to write packets out to a specific node (CC2538)  and read packets from different CC2538 nodes.  

Thanks in advance,

Brandon