Other Parts Discussed in Thread: CC2530
Hi all
i know it is unbelievable about this phenomenon。 but i would like to share my debug process、
first time i add two private function about initial UART0 and receive data .
void SerialInit(void)
{
halUARTCfg_t uartconfig;
uartconfig.configured = TRUE;
uartconfig.baudRate = FS_UART_DEFAULT_BAUDRATE;// 115200
uartconfig.flowControl = FALSE;
uartconfig.flowControlThreshold = 5;
uartconfig.rx.maxBufSize = 128;
uartconfig.tx.maxBufSize = 128;
uartconfig.idleTimeout = 6;
uartconfig.intEnable = TRUE;
uartconfig.callBackFunc = SerialCallBackFunc;
HalUARTOpen(0,&uartconfig);
}
/**
**FUNCNAME SerialCallBackFunc
**/
void SerialCallBackFunc(uint8 port, uint8 event)
{
unsigned char rcvdata[MSG_UARTRX_MAXLEN];
unsigned int rcvlength = 0x00;
osal_memset( rcvdata,0,sizeof(char)*MSG_UARTRX_MAXLEN);
ch = Hal_UART_RxBufLen(port);
rcvlength = HalUARTRead(0,rcvdata,ch);
HalUARTWrite(0,rcvdata, ch);
URX0IF = 0;
}
and i add those function in APP initial function
void zclSampleDoorLock_Init( byte task_id )
{
......
SerialInit();
HalUARTWrite(0,"12",sizeof("12"));
}
when i sending 22byte HEX data from PC side to CC2530, i trace the code one by one
Sending data :“ 00 11 22 33 44 55 66 77 88 99 AA BB CC DD EE FF 12 23 56 45 78 89 ”
PC side RX Data : "00 22 33 44 55 66 77 88 99 AA BB CC DD EE FF 12 23 56 45 78 89"
lose the second byte , no matter how long or how short the data i test to send.
trace receive data from PC side , and the data length is right .
and data is also right
then i trace the code in HalUARTWriteDMA
altough the txBuf data is also same with RX.
but PC side Only receive 21Byte data, and nomatter how long and how stort the data is , it was always lose the second byte
BR