This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC13xx with contiki 3.0 debug message & default channel



Dear All,

I am using SmartRF06 Evaluation board and  CC13xx EM with contiki 3.0 to develop my application.

But now I have encountered  two problems . 

1.  How to print debug messages to uart ?

    

2.  Can I run my app with RFband from 480.1 Mhz to 485.5 Mhz ?   

     I  have modified my code as below:

file: Dot-15-4g.h

   

#define DOT_15_4G_FREQUENCY_BAND_ID DOT_15_4G_FREQUENCY_BAND_470

#define DOT_15_4G_CHANNEL_MAX 675 
#define DOT_15_4G_CHANNEL_SPACING 8 
#define DOT_15_4G_CHAN0_FREQUENCY 480100 
#define PROP_MODE_CONF_LO_DIVIDER 0x0A

Thanks.