This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Hi Nodal Count Zigbee Application

We have an application that requires up to approximately 1000 nodes. Each node may be located up to 30 meter from the adjacent node in a 25 x 40 grid.  

We would like to be able to receive a small amount of environmental status information from each node every hour or so, in a demand-request fashion. The status information requirement is small, a 100 bytes or so.   We would like to be able to individually address each unit as well as be able to broadcast to all units.

Node cost needs to be $5 ish at 10K pieces.

Will the Chip Con Zigbee Pro Stack on a CC253x support this application?

Please let me know if this would be TI’s recommended solution or if there is a better solution.

 

Thanks in advance!