Hi all,
i initial a UART by mysel (do not using MT) like below :
ps:HAL_UART_DMA == 1
void SerialInit(void)
{
halUARTCfg_t uartconfig;
uartconfig.configured = TRUE;
uartconfig.baudRate = FS_UART_DEFAULT_BAUDRATE;//57600
uartconfig.flowControl = FALSE;
uartconfig.flowControlThreshold = 5;
uartconfig.rx.maxBufSize = 128;
uartconfig.tx.maxBufSize = 128;
uartconfig.idleTimeout = 6;
uartconfig.intEnable = TRUE;
uartconfig.callBackFunc =FS_UartProcessZToolData;//SerialCallBackFunc;
HalUARTOpen(0,&uartconfig);
}
when the device do not joined the network, the UART was worked. there is not any problem with TX and RX。
when the device joined the network ,and working under PM2 mode which Poll Rate was set as 20s.
and i found that the UART Tx was not working well, when i using HalUARTWrite() to sending a array , it seems that it was interrupted
by "someone"
TX array :0xEF 01 ff ff ff ff 01 03 01 00 05
Codeing:
uint8 AttachData[12]={0xEF,0x01,0xFF,0xFF,0xFF,0xFF,0x01,0x00,0x03,0x01,0x00,0x05};
HalUARTWrite(0,AttachData, 12 );
what is matter of the UART ?