This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ZigBee network

Other Parts Discussed in Thread: CC2530, CC2630, CC2538, CC2650

I am planning to make a ZigBee network and i have some doubts about the right TI chips to use.
1 - That Network will have 30 end devices (ZED) and one gateway that receives the data from all the 30 nodes. This gateway has also to communicate with an GSM/GPRS module. My question is for the ZED design the CC2630 seems like a perfect choice, but for the gateway it seems to have less memory than necessary. So, can I use the CC2530 or the CC2538 for this purpose or do I need to add an extra uC to complete the task (an MSP430 for example)? All the network devices will be battery powered, so the energy efficiency is very important.
2 - For the gateway I would appreciate to have a wake-on-radio device.
4 - If I choose any of the products above, how can I upload the software to the chips? Which ISP do I need?
Thank you very much.
Miguel