This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2630 EDGE ROUTER

Other Parts Discussed in Thread: CC2630, CC2650

HI,

I am working on a project which will use the CC2630 as nodes in a 6Lowpan network, I would like to use the CC2630 as part of the Edge router connected to a WIFI device.

1) Can the CC2630 work with Contiki to provide a SOC solution ?  passing the packets to the WIFI chip (with built in M4 cortex so no additional processing would be required from the CC2630 for the WIFI).

Regards