Other Parts Discussed in Thread: CC1310, CC1350
Dear All,
I am using TI cc1310 with contiki to print message via uart.
I built the hello-world example to test uart.
But it didn't print anything.
It's working in smartRF06+CC13xxEM.
I have modified the uart IO definition board.h of cc13xx module .
6LoWPAN\contiki\trunk\platform\srf06-cc26xx\srf06\cc13xx
From:
#define BOARD_IOID_UART_RX IOID_2 //evm board
#define BOARD_IOID_UART_TX IOID_3
To
#define BOARD_IOID_UART_RX IOID_2//CC1350 UART Rx
#define BOARD_IOID_UART_TX IOID_1 //CC1350 UART Tx
Did I miss something?
Can someone advise me how to correct it?
Thanks.