This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Possible that Zigbee-Device CC2530 working in different Networks without re-comissioning?

Hello there,

Im working on a lighting-network with CC2530, therefore I use the given ZLL-Gateway and the Zlight2.  

Im new in Zigbee-networking...

Im using 3-4 ZLL-Gateways with the Samplebridge(Coordinator).(Only one at same time)

If my Zigbee-devices are used with another ZLL-Gateway I have to reset them and have to do a new classical comissioning to join the network of the other coordinator.

So my question:

Is it possible to make the Samplebridge(Coordinator) exact the same as the other Samplebridges so that my ZDevices dont have to do a new comissioning and "feel" like they are in the same network?

Any Ideas?

Same Pan-ID?

Thank you in advance for your Help...Im working on this problem for too long :/

best regards