Other Parts Discussed in Thread: CC2650, CC2630, CC2538, Z-STACK
Hi,
I would like to know if the new generation ZigBee devices, I.E CC2630, CC2650, CC2538, can work in a network driven by a much older CC2480 (ZigBee Stack from 2006?). For example:
Can a CC2630 (as ZNP) join and communicate with a CC2480 (as ZNP)?
Note than in all cases, the CCxxxx devices are used as ZNP via SPI using SimpleAPI.
The ZigBee stack has obviously evolved and improved since 2006, but are the latest releases backwards compatible?
Or is it a case of changes to SimpleAPI which might make them incompatible?
Thank you