Hi All
there is a question about the CC2530 power consumption.
we made a private board which SCH is like below:
and there is always a peripheral circuit which is designed for detect the the vibration。
the first time we power on the device ,it seems OK that it only cost 10uA , but when it keeps power for longtime(maybe 5~6 minutes later )
it cost 200uA ~~~
Although the CC2530 is set in the PM3。
and i have do a test to make sure the power consumption of the peripheral circuit is OK。
nomatter how long does it run, it just cost 8~9 uA, and it is stable。
but i don't know what would cause the leakage current happen ?
BR