Hi all,
I'm currently testing and evaluting the Z-Stack with the Zlight2 development and I tried to operate the device with my philips hue hub. As the Hue bridge and Z-Stack are ZLL cerified, I thought that everything will work together. But after I have joined the device to an existing ZLL network via Touchlink (original ZLL Master Key was used), the device is detected by an Zigbee-Analyzer in the same network and the Philips Hue bridge does not find an valid lamp.
I took a look at the SimpleDescriptor of all devices in the network and saw that the ZLight uses HomeAutomation profile and all other devices (Philips Livining Color, Hue White) uses ZLL Profile. Maybe this is the difference?
So, my question is : Should the ZLight device (and the Z-Stack Lighting 1.0.2 with ZLL_1_0_HUB_COMPATIBILITY enable) be compatible with the Hue Hub?
Thanks in advance.
Best Regards,
Stefan