Other Parts Discussed in Thread: Z-STACK, CC2531, CC2530, CC2531EMK, CC2530EMK, CC2592
Hello,
I am having an issue with device association to the coordinator.
I have an device with IEEE address 00:12:4b:00:04:17:14:95. Now this device needs to be connected to coordinator. But instead it connects to the device which is already in the network i.e.IEEE address as 00:12:4b:00:03:e9:b0:53. and also it does not reflect on coordinator.
Here both devices are router.
I have attached the Sniffer file here.
What could be the problem here?
Device Association problem.zip
Regards,
Ajit Wadekar