Other Parts Discussed in Thread: CC2650, TIMAC
I would like to start a simple project on sensortag with cc2650.
I need to transmit/receive a simple ieee802.15.4 message on a defined channel with defined panId and address.
The other peer is a XBee connected to PC.
Is there a simple source code to perform a simple transmission and reception?
I'm going thru cc26xxware, timac and contiki, but they are too complicated for my needs, I don't want to import wagon of source files.
I don't need a complete stack like TIMAC or Zigbee. Too complicated to study, implement and debug.
Thanks in advance!