This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Connecting UART with external Input and Output

Other Parts Discussed in Thread: CC2530, CC253

Dears , 

I want to connect and input ( Two wire Bus - each 16 Volt ) to UART of  SmartRF05EB board , does anyone can help me with how to connect them and to which ports from the board ? I already know that the UART port in EB is P0.2 pin 9 as RX and Pin 11 as TX but it just one RX and One TX , what should I do if I need to connect to two RX ? 

Thanks