Other Parts Discussed in Thread: Z-STACK
Hi,
I am working with Z-Stack 1.2.1 HA profile. I am facing a problem that when I send permit join, one of my routers is present in the network but it doesn't join the co-ordinator. I don't even have a sniffer log currently because this problem is not persistent, but I will surely update later.
To understand where I am going wrong I need to understand following things:
1) When a router joins a network in which api I can check the status?
2) What are the cases when a router is in the network but doesn't get added to the coordinator?
3) Which are the api's in Z-Stack through which I can debug the association procedure?
4) Are there any good blogs or posts through which I can understand the association procedure in Z-Stack thoroughly?
Also I am using SampleLight application for testing.