Other Parts Discussed in Thread: CC2531, CC2650STK, Z-STACK, CC2650
Hi,
I'm trying to bind the sample switch on the SensorTag with a ZTool + cc2531 based coordinator.
I followed the instructions in: here and also in the TI forum, but until now I never succeeded, and I really can't figure it out why.
Here is my setup:
SensorTag with sample application, disabled HOLD_AUTO_START, ZCL_EZMODE, and NV_RESTORE.
ZStack version 1.2.2a.
The SensorTag associates and can manually send data, but cant' bind.
I have attached the log of ZTool.
The really strange thing is that when I send the binding command, the SensorTag seems to reply ZDP_TABLE_FULL, even though the table is (or should be) empty. In fact, I have erased the tag and reprogrammed it, and if try to unbind it, the sensortag replies "entry not found".
Also, if I issue the ZDO_MGMT_BIND_REQ, the reply is ZDP_NOT_PERMITTED...
Did I miss something?
Any help would really be appreciated :)
<RX>12:20:26.79 COM10 ZDO_END_DEVICE_ANNCE_IND (0x45C1)
SrcAddr: 0x10B3
NwkAddr: 0x10B3
IEEEAddr: 0x00124B00079ED581
Capabilities: 0x80
<TX>12:21:03.36 COM10 ZDO_BIND_REQ (0x2521)
DstAddr: 0x10B3
SrcAddress: 0x00124B00079ED581
SrcEndpoint: 0x08
ClusterID: 0x0006
BindAddrMode: 0x03 (ADDRESS_64_BIT) (0x3)
BindAddr: ..K..Zf. (0x00, 0x12, 0x4B, 0x00, 0x01, 0x5A, 0x66, 0xE6)
BindEndpoint: 0x07
<RX>12:21:03.38 COM10 ZDO_BIND_REQ_SRSP (0x6521)
Status: afStatus_SUCCESS (0x0)
<RX>12:21:12.15 COM10 ZDO_BIND_RSP (0x45A1)
SrcAddr: 0x10B3
Status: 140 (0x8C)
<TX>12:23:16.76 COM10 ZDO_BIND_REQ (0x2521)
DstAddr: 0x10B3
SrcAddress: 0x00124B00079ED581
SrcEndpoint: 0x09
ClusterID: 0x0420
BindAddrMode: 0x03 (ADDRESS_64_BIT) (0x3)
BindAddr: ..K..Zf. (0x00, 0x12, 0x4B, 0x00, 0x01, 0x5A, 0x66, 0xE6)
BindEndpoint: 0x07
<RX>12:23:16.77 COM10 ZDO_BIND_REQ_SRSP (0x6521)
Status: afStatus_SUCCESS (0x0)
<RX>12:23:22.37 COM10 ZDO_BIND_RSP (0x45A1)
SrcAddr: 0x10B3
Status: 140 (0x8C)
<TX>12:25:20.4 COM10 ZDO_MGMT_BIND_REQ (0x2533)
DstAddr: 0x10B3
StartIndex: 0x00
<RX>12:25:20.41 COM10 ZDO_MGMT_BIND_REQ_SRSP (0x6533)
Status: SUCCESS (0x0)
<RX>12:25:22.59 COM10 ZDO_MGMT_BIND_RSP (0x45B3)
SrcAddr: 0x10B3
Status: 139 (0x8B)
BindingTableEntries: 0x00
StartIndex: 0x00
BindingTableListCount: 0x00
BindingTableList:
<TX>12:27:25.81 COM10 ZDO_UNBIND_REQ (0x2522)
DstAddr: 0x10B3
SrcAddress: 0x00124B00079ED581
SrcEndpoint: 0x09
ClusterID: 0x0420
DstAddrMode: 0x03 (ADDRESS_64_BIT) (0x3)
DstAddress: ..K..Zf. (0x00, 0x12, 0x4B, 0x00, 0x01, 0x5A, 0x66, 0xE6)
DstEndpoint: 0x07
<RX>12:27:29.53 COM10 ZDO_UNBIND_RSP (0x45A2)
SrcAddr: 0x10B3
Status: ZDP_NO_ENTRY (0x88)