Hi,
I was working with zstack at cc2538 microcntroller for Home Automation.
I want to develop a Linux based gateway for my zigbee network
so can any one help me from where to start for the gateway application
Thanks in Advance,
Sibin Sunny
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi YiKai,
Is that means download ZNP firmware into CC2538 and then connect CC2538 to linux Host platform via UART.
and then, run the Zstack linux gateway application on linux HOST platform, and it will communicate CC2538 automatically ???