This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ZigBee Simple API Example (command sequence) for CC2530

Other Parts Discussed in Thread: Z-STACK, CC2530

Hi,

I'm using the CC2530 and interfacing it with the MSP432 (ZAP). I'm using the Z-Stack Mesh to flash the CC2530.  I have UART communication established between the two. I'd like to start using the simple API since I'm porting all the code and commands to the MSP432. Is there a current document or code example that indicates the proper way to establish a PAN (coordinator) and router/end device using the simple API? The proper sequence for configuration using this API would be of much help.

Thanks,

-Edgar