Other Parts Discussed in Thread: CC2650, Z-STACK
Dear All,
We are trying to use CC2650 Multiprotocol Zigbee chip with our ARM 64-bit processor platform using UART/SPI/I2C interfaced.
For that we found the Z-Stack_Linux_Gateway-1.0.1 HA Gateway application PART numbered suitable.
(www.ti.com/.../z-stack :Z-Stack™Linux Ubuntu Gateway installer)
We need to know that this gateway application will suit/run for the interface UART/SPI/I2C between CC2650 ZigBee and our ARM 64-bit processor.
We found that the server arm applications(servers/GATEWAY_SRVR_arm, NPI_lnx_arm_server, NWKMGR_SRVR_arm, OTA_SRVR_arm and ZLSZNP_arm) are compiled/built for 32-bit ARM platform only,
but we need to build the server applications for 64-bit ARM platform.
Also we are unable find the source code for these GW server ARM applications for recompiling for our 64-bit ARM platform.
So will these server applications will work in our 64-bit arm platform? If so how to recompile and/or run!!
Also please let us know how to tune the above server applications for UART/SPI/I2C DevPort instead of CDC-UART over USB?
Our Setup will be:
[ 64-Bit ARM Processor <- -> UART/SPI/I2C Controller ] <====> TI's CC2650(Zigbee Coordinator/Router)
Thanks,
Ashok