Hi all :
there are 4 ZEDs ,1 ZR and 1 ZC in the network.
those ZEDs were all connect to the ZR , and the ZR connect the ZC。
i set a timer to sending the Active EP request from ZR to ZC again and again to checking the link state.
if(events & NETLINK_CHECK_EVT)
{
if(Being_Link == FALSE)
{
#ifdef LEDShow
HalLedSet ( HAL_LED_2, HAL_LED_MODE_OFF);
if(!BasicReset)
HalLedBlink ( HAL_LED_1, 0,LOST_NETWROK_FLASH, LOST_NETWROK_CYCLE );
#endif
}
else
{
#ifdef LEDShow
HalLedSet ( HAL_LED_1 | HAL_LED_2, HAL_LED_MODE_OFF);
#endif
}
if(FailedLinkCnt >= LoseLinkCnt_Limit)
{
Being_Link = FALSE;
FailedLinkCnt =0;
}
else
{
FailedLinkCnt++;
}
ZDP_ActiveEPReq(&Coordinator_dstAddr,Coordinator_dstAddr.addr.shortAddr,0);
osal_start_timerEx( zclVrouter_TaskID, NETLINK_CHECK_EVT, NETLINK_CHECK_CYCLE);//8second
return ( events ^ NETLINK_CHECK_EVT );
}
this network running 30~40 minutes latter, i found that all ZEDs and ZR were “lose connect” with ZC.
Those ZED sent a Msg to ZC via ZR , but ZR receive it and didn't resend to ZC.
and there is not any ACtive EP request more....
here is the log :ZR lose connect with ZC.rar