Hello,
currently I am designing a zigbee development board with the CC2480. I want to use the same antenna design which is used on the usb dongle reference design with the CC2511 chip.
The antenna dimensions are clear, because well described in the application note AN043. The question is the matching circuit. The matching circuit in the application note for the CC2480 varies to the matching circuit of the CC2511.
Can I use the matching circuit and all dimensions/isolates described in the gerber of the CC2511 for the CC2480? If yes, how I can integrate the TXRX_Switch line?
Thanks in advance,
Florian