Hi guys,
I am kind of new to IoT solution development and want to know some information about some points that I got stuck with. Now I want to develop solution using ZigBee technology, let us say a light sensor and an electrical switch both connected to a gateway.
My questions are:
1. For the gateway, is the reference design of say CC2530 usable for making commercial production of gateway? Like is it enough or I need to modify it and work with its hardware more. (if i need more knowledge about this part link me to courses or PDFs)
2. For the part of sensor and electrical switch, are there any reference designs aswell or for those I have to start from scratch?
3. Is the development kit of CC2530 mainly a gateway that I can use to connect with different devices to insure the structure is working before production?
4. Is there a gateway reference design for CC2650 or it is not made to be used in a gateway?
I am sorry for asking a lot but I am very interested about this topic and I am unable to find direct information that fills my questions.
Thanks in advance...