This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AF_DataRequest AND TransID~

Hello

for the method

afStatus_t AF_DataRequest( afAddrType_t *dstAddr, endPointDesc_t *srcEP,
                           uint16 cID, uint16 len, uint8 *buf, uint8 *transID,
                           uint8 options, uint8 radius )

 

When EC AND ED connected.

ED send 10 words to EC then reboot~

And ED still send message to EC.

But it must 11th words be shown.

Because EC rember ED already sent 10 words.

How can I improve it?

 

Thank you~