Other Parts Discussed in Thread: TPS3823, CC2538
Hi all,
I'm trying to use the TPS3823 WDT with the CC2538 to supervise a security reset, but I have a problem that I usually program the CC2538 over BSL (UART), and when TSP3823 is mounted I can't program the MCU. Now the circuit design is the same as the datasheet of the WDT and I'm programming the MCU over BSL with an USB connection.
Can you recommend any design circuit to disable the WDT when the programming supply (USB) is connected or something like that?
Thanks!
Toni